Meet space requirements and energy codes with GreenMAX DRC Wired.
The Challenge
A Cambridge, Massachusetts. Biotech shared lab facility renovated its seven-story brick building to accommodate lab space and meet 2018 IECC code requirements.
Cambridge is a hub for laboratory and office space, and this existing, older building was renovated to meet the demand. A new high-rise glass lab tower was built onto it along with a connecting glass sky bridge.
The Installation
Leviton worked with the deisgn team and electrical contractor to provide a distributed lighting control system that met 2018 IECC energy code requirements.GreenMAX DRC Room Controllers, Smart Packs, and Digital Sensors were installed along with standalone occupancy sensors.
The Solution
GreenMAX DRC Room Controllers and Smart Packs were installed for switching and 0-10V dimming control throughout the building.The GreenMAX DRC Digital Sensors in the glass sky bridge provide occupancy sensing, daylight harvesting, and continual dimming. Leviton standalone sensors were installed in the offices and labs to ensure the lights remained ON when occupied and OFF when vacant.
GreenMAX DRC Room Controllers(s’ouvre dans un nouvel onglet)
Serve as the “brain” of any GreenMAX DRC Room Control System by coordinating the energy management functions within the room. Each room requires a room controller to connect with components such as DRC Smart Packs, and sensors.
GreenMAX DRC Smart Packs
GreenMAX DRC Smart Packs(s’ouvre dans un nouvel onglet) enable switching and 0-10V dimming control of a single zone of fixtures, allowing for a simplified, low-cost, distributed control solution. The smart packs use distributed relays to control multiple fixtures in a zone or enable plug load control, eliminating the need to run wires back to the panel. Smart Packs can be used as a normal or emergency relay, or as a remote relay with the GreenMAX system.
GreenMAX DRC Digital Sensors
The OSR05s(s’ouvre dans un nouvel onglet) directly incorporate occupancy/vacancy and daylight sensing into the GreenMAX DRC system. The Sensor integrates a PIR occupancy/vacancy sensor with a daylight-sensing photocell, providing more capabilities while requiring less equipment and wiring.
Standlone Sensors
The OSC20(s’ouvre dans un nouvel onglet) combines the benefits of both PIR and U/S technologies for unrivaled performance and reliability. The self-adjusting microprocessor continually analyzes, evaluates, and adjusts the sensitivity and time delay to maximize performance.
Leviton offers spec-ready lighting and control solutions for laboratory and office applications for seamless installations and energy savings.
Learn more at Leviton.com/GreenMAXDRC(s’ouvre dans un nouvel onglet).